Viewing Details of Containerized Applications

You can view information about the Docker images or Helm charts included in a download package from the download package’s Download List page. Available information includes a digest as well as the command for downloading the image or chart from the Revenera registry.

Note:Use the instructions in Viewing Containerized Applications to locate Docker images and Helm charts that are available for you to download

To view details about Docker images and Helm charts in the End-User Portal

On the Download List page, do either of the following:

In the Container Images section
Click the + sign for the image for which you want to display details.
Point to the icon in the Pull Command column to display the pull command used for downloading the image from the Revenera registry.
In the Helm Charts section
The Charts tab displays a description, version and digest for each chart.
Point to the icon in the Pull Command column to display the pull command used for downloading the chart from the Revenera registry.

See Also