Downloading Helm Charts

To pull an image from the Revenera registry

1. Log in to the Revenera registry, as described in Logging in to the Revenera Registry.
2. In a terminal window on the client machine running Helm, use a command like the following to pull an image from the Revenera registry:

helm pull <repo-name><chart>

The following shows an example command:

helm pull demo-repo demo-chart

See Also