Downloading Docker Images

To pull an image from the Revenera registry

1. Log in to the Revenera registry, as described in Logging in to the Revenera Registry.
2. In a terminal window on the client machine running Docker, use a command like the following to pull an image from the Revenera registry:

docker pull <registry-hostname>/<project-name>/<image>:<tag>

The following shows an example command:

docker pull container-registry.uat-1234.revenera.com/demo-project/new-demo-image:6.0

See Also